Cancel
Showing results for 
Search instead for 
Did you mean: 

Need an idea with Worker

Hello all,

 

I have various machines and worker carries athe part away. I want to achieve a situation where the machines automatically gets the highest prority where the worker is located and priority resets to 0 the moment worker removed all the parts from the machines. similarly when the worker moves to other machine the other machine gets the highest priority until the machine is again empty.

Can someone suggest me some attribute of worker that I can use to achieve this?

 

Thanks in Advance!!!

1 REPLY 1

Betreff: Need an idea with Worker

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Sleeping-Buddha,

 

you can use the Importer controls. in the release control, you can reduce the priority of a Station. 

But how did you set the priority of a request to a higher value? Which event would you like to use for this?

 

Hope this helps.

 

Regards

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution