Cancel
Showing results for 
Search instead for 
Did you mean: 

Need help to understand few things

Valued Contributor
Valued Contributor

Can anyone tell what is the significance of the Green box and yellow box with dash as shown in the figure below.

 

2 REPLIES 2

Re: Need help to understand few things

Siemens Phenom Siemens Phenom
Siemens Phenom

A green box means that the value is inherited from the origin. So when you change the value at the origin it is automatically changed in all objects which are derived.

 

If you see the yellow box inheritance is turned off. This is done whenever you change a value in an instance.

 

You can turn on inheritance again by pressing this box.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Need help to understand few things

Valued Contributor
Valued Contributor
Thanks a lot..Smiley Happy