Cancel
Showing results for 
Search instead for 
Did you mean: 

Need help with SingleProc times

Creator
Creator

Hi, 

I am trying to simulate a process. In it I have 6 singleprocs. I would like to know if there was a way where i could regulate the time for each singleproc to be working. I put the total event time for 6 hours of simulation. But what I want to do is stop singleproc at 50minutes every hour and start singproc5 at 50minutes for just 10 minutes. And then back to the cycle. 

Would appreciate any kind of help.

Cheers

 

4 REPLIES 4

Re: Need help with SingleProc times

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Bipul,

you can stop a SingleProc by a pause.

Your problem fits very well on the object Trigger.

Please see the konfiguration of that object in the attached model for Plant Simulation 12.

I add an object TimeSequence for the purpose of validation.

Regards,

Peter

Re: Need help with SingleProc times

Creator
Creator

Hi thanks that was awesome. 

But how do i make SP5 start at 50: for 10: every hour. 

what attributes do i use for that. 

 

Best,

Bipul 

Re: Need help with SingleProc times

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Bipul,

 

please create a new Trigger. Deactivate the checkbox Repeat periodically. Set Active interval and Period length to 1:0:0.

On tab Values > Start Values set Default value to true. On Values > Contents insert two rows:

50:00 with false

1:00:00 with true

Run the simulation and check the result by using a TimeSequence.

Regards,

Peter

 

 

Re: Need help with SingleProc times

Creator
Creator

Thank you very much for the information. 

Much appreciated. 

 

best,

Bipul