Cancel
Showing results for 
Search instead for 
Did you mean: 

New at Plant Simulation 12 - Re-entry loop?

Experimenter
Experimenter

Hello, I need to do a re-entry loop.

 

Basically an entity needs to pass twice through machine 2 and machine 1 again. And then carry on to the final destination.

 

I think I need to give an attribute to that entity, but im stuck on the syntax. Smiley Sad Smiley Sad

3 REPLIES 3

Re: New at Plant Simulation 12 - Re-entry loop?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
can you post your model?
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: New at Plant Simulation 12 - Re-entry loop?

Experimenter
Experimenter

Sure thing!

 

Basically the Spheres have to pass SM2 (and the drying machine) two times (re-entry loop), before they may be transported to the next department(Drain).

 

I'm also concerned about the methods used for the buffers for the machines.

 

Sorry if this is basic stuff, really appreciate the help!

Re: New at Plant Simulation 12 - Re-entry loop?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
okay: look here
http://community.plm.automation.siemens.com/t5/Plant-Simulation-Forum/How-to-count-how-many-times-a-...

The approach is:
- define a user defined attribute in your MUs (e.g. counter, integer, start value=0, double click on the MUs in the class library --> tab user defined attributes)
- increase the counter in the entrance control of the dryingStation ( you access the MU with @ --> @.count:=@.count+1; )
- in the exit control you read the attribute count (@ is again the MU --> if @.count=1 then --> first time --> move to buffer --> else straight foreward):
is
do
if @.count=1 then
@.move(BufferS);
else
@.move;
end;
end;
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net