Cancel
Showing results for 
Search instead for 
Did you mean: 

No material movement between objects in VSM

Experimenter
Experimenter

Hi

 

I have a model which has 2 machines and a packing station to send it to the customer. I have introduced a kanban between machine 1 and a supermarket object i.e. my predecessor is a supermarket and my successor is a machine. This supermarket is in turn connected to the packing station. I have defined the customer requirement and supply frequency. Even the machine 1 has another supermarket object as a predecessor. Every thing is taking place properly except there is no material movement to the packing station from the supermarket object and the parts coming to this supermarket gets accumulated.

 

Can anyone tell me the reason for this.

 

Regards

Sujith

1 REPLY 1

Betreff: No material movement between objects in VSM

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Sujith,

 

can you please provide your model. This makes it easier for us to understand the behavior of the material flow and to find out why there is no material flow at all.

 

Regards

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution