Cancel
Showing results for 
Search instead for 
Did you mean: 

Numbers of objects in a model

Builder
Builder

Hi,

 

I would like to know if it's possible to know the number of objetcs in a model ? (the number that can be reached with a standard licence for exemple....)

 

thanks in advance,

 

Flo_M

5 REPLIES 5

Re: Numbers of objects in a model

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

try

 

print numOfLimitedObjects;

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Numbers of objects in a model

Builder
Builder

Isn't it the limit displayed with print numOfLimitedObjects ?

 

Because it says 55091, but if i had a method in the model, there is no difference with the count....

 

 

EDIT : BUT, if I had a singleproc, it says 55092 !

 

Is it this number that can be reached and limiting with a stantard licence of Plantsimulation?

Re: Numbers of objects in a model

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
have a look in the help --> content - Setting up and installing - Licensing Plant Simulation - Plant Simulation License Types

numOfLimitesObjects returns the number of counting objects for the license restrictions;
tableFiles and methods are not included
The standard license is restricted to 4.000 (limited) objects
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Numbers of objects in a model

Legend
Legend

please check "numnodes" in help menu

Sachin

Re: Numbers of objects in a model

Siemens Phenom Siemens Phenom
Siemens Phenom

The function 'numOfLimitedObjects' returns the number of counted objects. A method is not counted so it doesn't increase the number.

And yes, this is the number which is limited in a standard license.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.