Cancel
Showing results for 
Search instead for 
Did you mean: 

OPC server cannot connect for VC with Plant Simulation

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello,

I test for Virtual Commissioning with Plant Simulation as per presentation in User conference.(25_Guido_Gross_Siemens_Virtual Commissioning using Tecnomatix Plant Simulation_Usermeeeing_2015_approved).

I found some problem that I cannot download to device.

I think that issue from OPC Server status is not ok. (see in attached file)

How to solve this issue?

 

Thank you for the help in advance

Jeerawut R.

 

Download to device.jpgStation Configuration.jpgOPC Scout.jpg

3 REPLIES 3

Re: OPC server cannot connect for VC with Plant Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Jeerawut,

 

look at the screenshot of the station configuration editor. There you will see, that the OPC serv er isn't configured in the right way. May be the problem is caused by different positions? Look at slide 18 of 'Virtual commissioning' from user meeting last year. There you will see what I mean with 'correct position'.

 

I attached the slides to this post.

 

Reagrds

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: OPC server cannot connect for VC with Plant Simulation

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi GG,

 

Thank you for your information.

I already Compile as page18. It show same as that page.

But I have some doubt about page 16. My OPC server did not show status same as that page.

And For page 20, I cannot search for device.

How to solve about OPC server status?

 

Thank you & Regards,

Jeerawut R.

Re: OPC server cannot connect for VC with Plant Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Jeerawut,

 

make sure the slot position of the 'OPC server' and 'IE General' are the same, otherwise, the status will not be ok

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution