Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Object doesn't leave source

Creator
Creator

After the 1st Source Object, the others objects don't go to the PickUpStation.

 

On version 12, it was working, and after the update, it stopped working. Do we need to change something to it works?

 

Thanks

Pedro

4 REPLIES 4

Re: Object doesn't leave source

Phenom
Phenom

I've updated the source(class)  settings

 

Now it should work again (s.attachment)

Re: Object doesn't leave source

Creator
Creator

Hi,

We have the version 13.2.2 and you have 13.2.3.

 

And it didn't work.

How did you do this update?

 

Thanks

 

 

Capture.PNG

 


@simulator wrote:

I've updated the source(class)  settings

 

Now it should work again (s.attachment)


 

Re: Object doesn't leave source

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
deactivate in the PickAndPlace - Entrance Control - before Actions, then it works in V. 14 , this causes the problem

if you connect B1F29 with a connector with the pickAndPlace (as Exit), you dont Need a Control in the PickAndPlace
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Object doesn't leave source

Phenom
Phenom

@phcella

update meant ,  I set the count parameter to 1 pressed "accept" and set it back to -1

 

 

Unbenannt.PNG