Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Object "was already deleted"

Pioneer
Pioneer

Hello everybody,

 

currently I'm having trouble deleting an object. Once I try to delete it, a notification "The object was already deleted" is shown. The object remains in the model. When trying to delete it using <object>.deleteObject, PS crashes du to some Access Violation.

 

Did that problem occur to anyone before?

 

As always, thanks a lot,

 

Tim

1 REPLY 1

Re: Object "was already deleted"

Siemens Phenom Siemens Phenom
Siemens Phenom

It can happen that an object that you delete will not be deleted immediately. This usually happens when the destructor is being suspended or when you are debugging the destructor control.

 

The program should of course not crash. If you upload a model with which I can reproduce the crash, I will investigate the problem.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.