Cancel
Showing results for 
Search instead for 
Did you mean: 

Opcclassic error

Creator
Creator

Dear Sir

I am trying to create a connection between Opcclassic as a client with Plc server.  But when i just trying to enter the server its start giving an invalid string error Pictures are attached below. Do we need any method as well to work my model exactly with the existing system because working as a client to creating a server. I am using a 14.0 version

Model and Picture attached below.

 

 

Thanks

Malik 

1 REPLY 1

Re: Opcclassic error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Malik1,

 

The string you enter looks like a OPC UA connection.

For OPC classic you have to enter the class name of your OPC server.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.