Cancel
Showing results for 
Search instead for 
Did you mean: 

Open PDF file automatically on opening a project

Valued Contributor
Valued Contributor

Hello,

 

When I open the provided example "DeliveryConcept" I get a message box "Do you want to open a description of the model as an Adobe Acrobat Document?" and I get the documentation for this project.

 

I would like do do the the same in my Plant Simulation project, how can I achieve that ?

 

Thanks in advance

2 REPLIES 2

Re: Open PDF file automatically on opening a project

Phenom
Phenom

With an implemented autoexec method you can start a code execution immediately after model load

 

With startExtProc(...) can open the acrobat reader from Plant simulation.

Re: Open PDF file automatically on opening a project

Another possibility is to use the FileLink object and reference or embed the PDF file.

 

FileLink.PNG