Cancel
Showing results for 
Search instead for 
Did you mean: 

Open a model with an older version

Legend
Legend

Hello everyone,

 

I've built a modelwith the version 13.0. Then I saved it with the version 13.2 and finally I noticed some dysfunctions with this version and I'd like to come back to the old version. 

 

There is anyway to do it by my self or should I contact GTAC ? 

 

Thank you very much. 

 

Best regards
O.C

2 REPLIES 2

Re: Open a model with an older version

Siemens Phenom Siemens Phenom
Siemens Phenom

When you load a model from an old version, Plant Simulation tells you that if you save it with the new version, you can no longer open it with the old version. It even tells you this once again, when you actually save it.

The more interesting question is: what are the "dysfunctions"? Normally an old model should work perfectly in a new version.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Open a model with an older version

Legend
Legend
Hello Michael,

Sorry for the delay !

I'd like to thank you for your comment ! I finally fixed the problem, it was an issue related to my graphic card. Kind of crazy !

Thank you very much !

BR
OC