Cancel
Showing results for 
Search instead for 
Did you mean: 

Output of a changed delivery processess

Creator
Creator

Hallo dear fellows,

 

I set up a basic model of a changed delivery processes.

 

The model should generate the changed data such like new delivery date/quantity.

 

the input are:

- plan_quantity_dEmp

- plan_divery_date  -> should refer to the simulation time

- delivry normal distribution -> z_noraml

 

- difference_plan_new_dlvry_time

- difference_pland_new_dlvry_quantity

 

- difference_new_JITcalloff_dlvry_time

- difference_new_JITcalloff_dlvry_quantity

 

 

the output should be gathered in output table by programming a controll method.

 

- new_dlvry_date

- new_dlvery_quantity

- JITcalloff_date

- JITcalloff_quantity

 

because I am quite a new hand on this simulation tool, so there is still a problem with filling out the output table. It means, I let the model run, but happes nothing with the output table. There must be lack of a logic connection between the elements that I can not find. So if some of you can tell, that would be great !

 

Thanks a lot in advance !

 

Best regards

 

J. Inkheart

 

1 REPLY

Re: Output of a changed delivery processess

Siemens Phenom Siemens Phenom
Siemens Phenom

Your model contains at least two issues:
XXX.png

  1. Objects showing a cyan dot do have <Obj>.EntranceLocked=true, most likely your reset should set them back to false, otherwise no part ever will reach a drain.
  2. Data_Gathering is syntactically wrong, this makes me believe you do not use the debugger optimally. (Before you write any line of code in a method, just set a breakpoint and make sure the method is called as expected. After that you may develop your code, supported by the debugger - your most efficient development tool.)

 


Regards

Always consider using the AttributeExplorer!