Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

PC shutdown after ExperimentManager finished?

Pioneer
Pioneer

Hey there,

is it possible to force an automatic shutdown of the PC when all experiments are finished?

So save model, save outcomes --> shutdown PC

1 REPLY 1

Re: PC shutdown after ExperimentManager finished?

Phenom
Phenom

I guess you can run  the shutdown

 

through the simtalk method startExtProc ("cmd /C shutdown /t timeOut").

 

Make sure , everything is completely saved before running the method.

 

For startExtProc / shutdown details look at Plant simulation help /

 

DOS help in DOS window