Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Pack and Go to read Data from Excel

Legend
Legend

Hi all,

 

in my real model I load paramters from an Excel sheet into a tablefile.

This run fine using the plantsim software.

 

As this model is supposed to be run as standalone, I create a packandgo.

However reading the Excel file sheet is not possible.

The Excel is located in the same folder as the executable on the disk.

 

 

Kind regards

Marco

 

12 REPLIES 12

Re: Pack and Go to read Data from Excel

Phenom
Phenom

data import- /export is not intended

 

for  pack & go - Plant Simulation models !

Re: Pack and Go to read Data from Excel

Siemens Phenom Siemens Phenom
Siemens Phenom

if any interface would be open in a pack&go we could stop selling PS, because one could do anything without a license ... sorry, but this is not our business model


Regards

Always consider using the AttributeExplorer!

Re: Pack and Go to read Data from Excel

Legend
Legend

Thanks for the update.

 

Our intention was to have a parametrization using real data from the existing production line.

So I let our management know that the simulation can only run on a PC with the license installed.

 

Regards

 

Re: Pack and Go to read Data from Excel

Siemens Phenom Siemens Phenom
Siemens Phenom

Please keep in mind just to have the need for a Runtime-License ... refer to help: Setting-Up and Starting > Plant Simulation License Types > Available Features of the Individual Licenses

 

Interface Package would not be required in your case.


Regards

Always consider using the AttributeExplorer!

Re: Pack and Go to read Data from Excel

Legend
Legend

Thanks for this info, now I have further questions.

Our company has purchased one license (development) installed on the network.

As a developer, IT installed the plant simulation (v13.1) on my workstation. I use this license for my development.

 

Is is possible to have anyone else to use this license without having the software installed for development ?

Other people want to run the model without making any changes to the graphics layout and code.

Or so we need another license ?

 

Regards

Marco

Re: Pack and Go to read Data from Excel

Phenom
Phenom

Have a look at the viewer license.

 

You can run ( but not modifiy) Plant Simulation models w/o a commercial license.

 

 

Unbenannt.PNG

Re: Pack and Go to read Data from Excel

Legend
Legend

The intention how to use the model I created is:

 

Development (Me) creates an executable, releases new version during further developement.

Provide an interface via Excel to allow parametrization

  • Setup and Process times of each workcell (=Single Proc)
  • Enabling for n workcells of a type to have multiple resources for the specific workpart. This allow to evaluate the change of efficiency on the whole production line.
  • Set amount of part per batch, process x batches
  • Set amount of workers (supply raw, do setup and maintenance) and part transportation AGV's

Anybody can run the model using the parametrization.

 

The question is now:

  • Shall we install plant simulation on specific workstations and let used run the model using the development license. We might need to purchase an additional normal (development) license.
  • Shall we have a run license to run the executable with the parametrization enabled.

 

 

Regards

Marco

 

Re: Pack and Go to read Data from Excel

Siemens Phenom Siemens Phenom
Siemens Phenom

If you want to be able to:

  • develop models (you) and perform experiments independently (your customer)
  • parameterize models freely (without being  limited to the options a Pack&Go provides)
  • exchange data via xlsx-files

an additional runtime-lic is to be recommended!

 

The Pack&Go is not intended to be used for "productive" simulations, main purpose of it is to allow:

  • running parametrized models
  • limited parameter changes (via checkmarks, radio buttons and drop-down lists)
  • exploring the model (better than by video)

 


Regards

Always consider using the AttributeExplorer!

Re: Pack and Go to read Data from Excel

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Marco,

To this end there is the Runtime license; it does not allow you to modify models (add/remove objects, SimTalk), but other than that it offers virtually all features and includes the interface package.

 

So, use your development license (e.g. Standard/Professional) to define te model structure and logic, data interfaces etc. Then this model can be opened and parametrized with a Runtime license.

 

This set-up is very common.


Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com