Cancel
Showing results for 
Search instead for 
Did you mean: 

Paint job: Different Products, different number of paint and dry cycles

Experimenter
Experimenter

Hello Community,

 

for my Master thesis I am simulating a paint job.

Overview.PNG

 

The painting time is 2,5h and the dry time is 8h. More or less every product has different times.

 

Some example times can be seen in t_calc. (Column "Number of paint jobs" shows how often is has to be painted and implys the same amount of drying processes)

I have to do it that way since I only get the total time of painting from the production.

 

In t_input I try to create a table where the different repetitions of Paint Job and Drying are shown, with the corresponding times (2,5h and 8h).

 

Now my question:

Since my list is in reality very long. I would like to automate the creation of the production table with a methode.

But I dont know how to do that.

I would like to have at t_input in the table, corresponding to the specific product, at "Attributname" the right amount of repetitions of Paint Job and Dying, with the corresponding time.

 

For example:

At t_calc:

Product 1.PNG

 

Product 1, Number of paint jobs = 5.

 

Therefore the table at t_input should look like:

How the table should look a like.PNG

 

I hope I could make my self clear.

I would really appreciate if someone could help me.

Thank you very much in advance.

 

Kind regards,

 

Chris

4 REPLIES 4

Re: Paint job: Different Products, different number of paint and dry cycles

Phenom
Phenom

I made some adjustments (s. m_inputcode, t_input))

 

 

 

Unbenannt.PNG

Re: Paint job: Different Products, different number of paint and dry cycles

Experimenter
Experimenter

Dear simulator,

 

thank you very much.

 

Unfortunately I have some more questions, concerning your solution.

 

Since there are now several e.g. "As" in the Input Table (t_input), does that mean I have several products A?

 

Because I meant to have one product A which needs several painting and drying processes. Therefore I thought I have to define the number of paint and drying jobs in the table "Attribute".

 

Thank you very much for your time.

 

Kind regards,

 

Chris

Re: Paint job: Different Products, different number of paint and dry cycles

Phenom
Phenom

I've added a count attribute and rearranged the layout.

 

Have a look

Re: Paint job: Different Products, different number of paint and dry cycles

Experimenter
Experimenter

Dear simulator,

 

thank you very much. That is exactly what I need.

 

Kind regards,

 

Chris