Cancel
Showing results for 
Search instead for 
Did you mean: 

Parallel Processing Problem

Valued Contributor
Valued Contributor

Hello All

 

I have a situation where in the worker loads two parts on to parallelproc1 from parallelproc and after every cycle ,the worker has to unload the two  parts simultaneously from parallelproc1 and place on the buffer1  and then load two new parts from parallelproc to parallelproc1.

 

I have the logic written but the model seem to be not working as per the scenario. I request anyone to look into the model and help me with it.

 

Kind Regards

Sujith

5 REPLIES 5

Betreff: Parallel Processing Problem

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Sujith,

 

On tab Exit of the ParallelProc you defined the target for the MUs as ParallelProc1. So every parts will be carried to this station.

 

Remove the target definition on tab Exit of the Parallelproc and define the target of the MU by setting attribute Destination of the MU.

 

Hope this will help.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Highlighted

Betreff: Parallel Processing Problem

Valued Contributor
Valued Contributor
Could you please send across the modified model as per the solution given
from your side. Because its not working,hope so i would have misunderstood.
It would be of great help.

Regards
Sujith

Betreff: Parallel Processing Problem

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Sujith,

 

soory, but I didn't have the model running, I just recognized that the move statement in your entrance control disturbs the behavior of the worker when carying part away is used.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Parallel Processing Problem

Valued Contributor
Valued Contributor

HI

 

The logic is not working, its behaving in a different manner

Betreff: Parallel Processing Problem

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Sujith,

 

attached you will find your model. The worker is carrying 2 Parts from ParallelProc to ParallelProc1 and afterwards 2 parts from PrallelProc1 to Buffer.

I removed all method call and only inserted to methods as you can see in the model.

 

Hope this will solve your problem.

 

Regards

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution