Cancel
Showing results for 
Search instead for 
Did you mean: 

Parallel proc with two entrance(raw),but produce one by one.

Experimenter
Experimenter

Hello PLM community,

I have a little problem!I have to create a parallel proc,which has two places for raw(materials),but can process only one part.I want to loading the two places,but then the machine start to process the both parts.I want to process them one by one.Can you help me?Thank you in advance!!!

 

Smiley Happy Smiley Happy Smiley Happy

2 REPLIES 2

Re: Parallel proc with two entrance(raw),but produce one by one.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

A simple approach could be to set a Cycle time or Recovery time on the ParallelProc and connect it to a SingleProc. Then set the Processing time of the ParallelProc to 0 and give the SingleProc the correct processing time. Your model will now accept MUs as long as the ParallelProc has place left, but only at specific intervals. Due to the SingleProc, MUs will be processed one-by-one.

 

You can make it more fancy with SimTalk, but this basic version should already work.

 


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Parallel proc with two entrance(raw),but produce one by one.

Experimenter
Experimenter
This proposed solution help me a lot.I done everything,like I want.Thank you for helping!