Cancel
Showing results for 
Search instead for 
Did you mean: 

ParallelStation animation line

Legend
Legend

He,

 

I want to use a parellelStation with 4 line animation. each station have a path.

 

I don't understand why the duration of the line animation is not linked to the procTime.

 

Is there a way to do that ?

 

Regards,

 

rpinon

8 REPLIES 8

Re: ParallelStation animation line

Phenom
Phenom

you can manually set the time (s.b.)

 

Through simtalk you can read out the animation path data

 

(_3D.MUAnimations.AnimationPathName.getTable(table) )

 

 

set the time per segment in the data table and then rewrite

(_3D.MUAnimations.AnimationPathName.setTable(table) )

 

the  path data.

 

 

 

Unbenannt.PNG

 

 

Re: ParallelStation animation line

Legend
Legend

Hi,

 

Thanks for your reply,

 

Your solution is a great around solution, but what if I want different procTime for each station in the parallelStation ?

 

Regards,

 

rpinon

Re: ParallelStation animation line

Phenom
Phenom
The solution is the same !

- read out the animation path data
- set the time per segment
- write back the animation data

Re: ParallelStation animation line

Legend
Legend

Oh Yes, I understand. It's because each station have a line animation.

 

Thanks, too bad that there is no built-in function to do that.

 

Regards,

 

rpinon

Re: ParallelStation animation line

Legend
Legend

On the other hand,

 

self.~._3D.MUAnimation.#1#1.getTable(tmpTable) 

Return an error : Syntax error near line 7 at '#'

 

means that I cannot get my MuAnimationPath....

Re: ParallelStation animation line

Phenom
Phenom

@ "Thanks, too bad that there is no built-in function to do that."

 

With which version are you modelling

 

until v13.2 the dedicated animation paths were

 

displayed (s.b.)

 

 

From v14.0 you have ( on top)

 

the possibility define an area  to automatically place the

 

MUs

 

Unbenannt.PNG

 

Re: ParallelStation animation line

Legend
Legend

I use the lastest version of plantSimulation with several hotFix so 14.1.2++

 

Yes I know that you can use the area. But I want path animation for each station.

Re: ParallelStation animation line

Phenom
Phenom
try

station._3d.MuAnimations.getAnimation("#1#1").getTable(tab)

or

station._3d.MuAnimations.getTable(tab)

for all animation paths