Cancel
Showing results for 
Search instead for 
Did you mean: 

Performance Issue

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hi!

 

I had some trouble getting my pointcloud to fully render and it got slightly better with a more powerful laptop so my reasoning made me to think that if I ran my simulation on a powerful stationary it would be all good.

 

Problem is that on a i9-7900X 3.3GHz, GeForce 1080Ti and 30Gb of RAM with Windows 10 64bit it runs horribly.

Is there any know issues with PlantSim and Core i9 or something to explain this?

 

Thanks in advance

10 REPLIES 10

Betreff: Performance Issue

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello ALilj,

So you're saying that the performance got worse with a more powerful hardware?

 

The Core i9 CPU together with the GeForce should be an ideal configuration.

One important hint is to put the point cloud onto a SSD drive. Since point clouds are in the area of GBs the read performance from the hard disk is usually the most critical bottle neck.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Betreff: Performance Issue

Phenom
Phenom

I assume you are posting about the 3D performance.

 

To put the 3D performance  in numbers. 

 

Select  the 3d window and press "F" to see the frames per second.

Betreff: Performance Issue

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Yes, 3D performance is lacking. I get 3.5-4 fps when running the simulation and running a camerapath through the plant. The model is not large either, about 100 m^2 in total.

Betreff: Performance Issue

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

I find it wierd too that it doesnt perform as well as it should do with this much computing power behind it. Both PlantSim and the point cloud is located on a SSD drive and I'm getting 3,5-4 fps when running the sim and running my camerapath.

Betreff: Performance Issue

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you tell me the file size of your point cloud?

 

I have a point cloud with 9GB file size and on my notebook (Core i7-6820HQ, NVidia Quadro M1000M, 1920x1080 screen resolution) I get a frame rate of ~23fps once the point cloud is fully loaded.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Betreff: Performance Issue

Phenom
Phenom

2-3 fps is too low

 

It should be roughly > 25 fps to get a non flickering move

 

I guess the graphics card is mainly designed / optimized  for  triangulated objects than points.

Betreff: Performance Issue

Siemens Phenom Siemens Phenom
Siemens Phenom

To be clear, I get a frame rate of ~23fps not ~2-3fps.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Betreff: Performance Issue

Phenom
Phenom

@ralf

 

the post was related to @ALilj performance values.

Betreff: Performance Issue

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

The pointcloud is on 213mb so cant be that either. Gonna have to look into it further but I thought I might as well check here if there were reported confirmed issues with the Kaby Lake architechture or something along those lines.

 

Thanks for all the responses