Cancel
Showing results for 
Search instead for 
Did you mean: 

Pick and Place Issue

Pioneer
Pioneer

Hi community, I have encountered an issue with a "kind of simple" Pick and Place setUp and I would like to read some feedback about it to find my way back into the workflow.

 

The scenario is the following:

 

The pick and place robot recieves a product from the source, then it takes it to A or B, whichever is free

(if both are free, then it must go to A)

 

Before going to "A" or "B", it needs to make a temporary stop at the station "TempStationA" or "TempStationB" (depending if it is going to A or B), then wait for the process in "TempStation" to be concluded, and then (Without having moved since the drop) take again the product and move it to its final destination.

 

 

2 REPLIES 2

Re: Pick and Place Issue

Legend
Legend

Hi,
I made a small example.
You can use it as a starting point.

Re: Pick and Place Issue

Pioneer
Pioneer

Thanks a lot, thats exactly what I needed