Cancel
Showing results for 
Search instead for 
Did you mean: 

Pick and Place doesnt work between 2 single processo

Valued Contributor
Valued Contributor

Hello,

 

I just tried simple disassembly line, I used Pick and place in between  2 single processors  but it seems not work.

during the simulation,  MU skipped P&P.. I am much curious what is problem..

So I attached my trial file,  please see the "Backgroundframe" frame..

 

Thank you in adavance,

 

2 REPLIES 2

Re: Pick and Place doesnt work between 2 single processo

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

please turn on the icon animation. Then you will see the turning of the p&p.

Without icon animation you will not see change of status (pause, failed,...) and the turning of objects P&P and turntable.

But in the event list you can see the time consuming. There are different times when the MU enters and leaves the P&P. So the P&P is not skipped.

 

Kind regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Pick and Place doesnt work between 2 single processo

Valued Contributor
Valued Contributor
Thanks a lot! Solved!