Cancel
Showing results for 
Search instead for 
Did you mean: 

Pick and Place strategy

Experimenter
Experimenter

Good day,

 

I need to simulate a pick and place robot that picks up parts in a buffer, moves them to a process and then moves the processed part to other buffer.

 

Captura.PNG

 

The process should be as follows:

 

Robot picks up MU at "in", moves that MU to "machine", before dropping the MU at "machine", picks up the previous MU from "machine" (double grip robot), drops the new MU, and then moves the previous processed MU to "out". 

 

Any suggestions?

 

Thanks in advance.

2 REPLIES 2

Re: Pick and Place strategy

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
one way is to use a "helping place" for the machine and load the new part to this place first.
like in this example:

http://www.bangsow.eu/detail_en.php?id=518
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Highlighted

Re: Pick and Place strategy

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

another option would be to use a parallel station instead of the single station to model your use case. Attached you can find a model where your application is implemented with a parallel station.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution