Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

PickAndPlace Control

Creator
Creator

Hello Community!

I need your help to go forward with my model. I would like to separate three parts: one part move to Washer1 or Washer2 (I have two washers due to capacity problem) and the carrier and the rest part on it I would like to move to Washer21 or to Washer22. After the washing process finished the original three parts should move forward together. 

Could you share a suggestion with me? (I have Plant Simulation v12). Thanks for your help you inadvance.

 

22 REPLIES 22

Re: PickAndPlace Control

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
could you make a small example? (as spp file!)
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: PickAndPlace Control

Creator
Creator

Dear Steffen,

 

attached you can find my semifinished model.

Thanks in advance your help.

Re: PickAndPlace Control

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you can use the exit control of the PickAndPlace

You could adress the part carrier, then you unload the first part, re-adress the carrier and send the PickAndPlace to the next buffer (setDestination), there you move the carrier itself

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: PickAndPlace Control

Creator
Creator

Hello Steffen,

 

thank you your answer. I tried to modify my model based on your solution, without success.

The part separation would be not the way as you solved.

I woul like to send all "Cylinderhead"s to direction PickAndPlace. Then the "Slipper_plate with the "Cover_Plate" to the PickAndPlace1. Washer1 and Washer2 washes only "Cylinderhead"s, Washer21 and Washer22 washes only "Slipper_plate"s with "Cover_Plate"s. After washing process, all Cylinderhead should placed back again to their original Slipper_plate and Cover_Plate.

Re: PickAndPlace Control

Creator
Creator

Hello,

 

attached you can find my model with some modification. As you can see on the attached picture the first cycle (the first picked parts) is working in the proper way, but the next part will move (all three items) to PickAndPlace1.

Could you correct my control methode according to the way what I described? 

At the end of conveyor belts the Cylinderhead has to be put on its original carrier (Slipper_plate). Could you show me this solution as well?

Thank you so much. 

Re: PickAndPlace Control

Phenom
Phenom

here's the code which should properly work.

 

is
do
	@.mu(1).move(PickAndPlace);
	wait 5.0;
	@.zielort:=PickAndPlace1;
	@.move(PickAndPlace1);
	
	
end;

 

 

I have inserted a 5 sec wait, so that the coverplate is not grabbed  by P&P1 before P&P handled the cylinderhead 

Re: PickAndPlace Control

Creator
Creator

Hi simulator,

 

thanks for your help!

Finally I would need to unite the parts again.

1. PaP3 should pick first the Slipper_plate and Cover_Plate from conveyor F11

2. then PaP3 should pick the Cylinderhead from conveyor F1

3. in the Placing assembly station the Cylinderhead will be placed to the Slipper_plate (Cover_Plate is already on it)

(Cylinderhead:1 should couple always with Slipper_plate:1 and Cove_Plate:1 ...etc.)

Could you please help me to solve this problem. (I am still beginner and I can learn to study the solutions)

Thank you in advance!

Attached the model (v12)

 

Re: PickAndPlace Control

Phenom
Phenom

1. unlock PaP3 exit (press inherit button)
2. create new method m02
3. add m02 as entry method to PaP3
3.1 add following code in m02

is
do
	if @.name="Cylinderhead" then
		?.setDestination(P1);
	else
		?.setDestination(P);
	end;
end;

 


4. set assembly list to "predecessor"
5. insert (predecessor=) 2, (count=) 1 in assembly list

 

Re: PickAndPlace Control

Creator
Creator

Hi simulator,

 

thank you very much your support!

It works.

 

BR

JLap