Cancel
Showing results for 
Search instead for 
Did you mean: 

PickAndPlace: rotation angle only in clockwise

Legend
Legend

Hi Guys,

it is possible to set rotation angle only in clockwise in PickAndPlace?


Thanks and Regards,
Nadin

2 REPLIES 2

Re: PickAndPlace: rotation angle only in clockwise

Siemens Phenom Siemens Phenom
Siemens Phenom

There is no simple setting to switch between rotating in the shortest direction and always rotating in a certain direction, if that is what you mean.

You might be able to tinker around with SimTalk in order to get a fixed rotation direction but before that, I would try to find out whether and if, why, this is needed.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: PickAndPlace: rotation angle only in clockwise

Legend
Legend

Hello PeterKomarek,

It is for no particular project.
I have assumed the traversing cart on way was the template for PickandPlace. That's why I thought this should go. I'm just wondering that I could not find this function.

thanks for this information.