Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Pie Chart to Track Variable Value

Hi All,

 

Relatively simple question (I think!).

 

I'm struggling to configure a Chart to display a Pie Chart which the value of a Variable and displays the values as a % of time over the Simulation. I usually use this chart set up on a Buffer, how this variable adds up the values of multiple buffers and therefore I would like this variable in a Pie Chart. I cannot quite seem to set it up properly.

 

Kind Regards,

Nathan

5 REPLIES 5

Re: Pie Chart to Track Variable Value

Phenom
Phenom

Do you mean something like this ?

 

 

Unbenannt.PNG

Re: Pie Chart to Track Variable Value

Hi Simulator,

 

Similar to that yes, but the Pie Charts I used to create from Buffers show how many parts are in the buffer as a percentage of time, like the example below. I would like the same Pie Chart format but it being generated from a Variable instead.

 

Pie Chart Example.png

Re: Pie Chart to Track Variable Value

Phenom
Phenom

Works also with variable objects

 

Unbenannt.PNG

Re: Pie Chart to Track Variable Value

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Open the variable, go to statistics, active and click on Chart. I believe this is what you wanted? 

 

 Capture.PNG

Re: Pie Chart to Track Variable Value

Thats the one! I didn't have Active turned on! Thanks very much