Cancel
Showing results for 
Search instead for 
Did you mean: 

Plant Crashes when I Create a MU on an Assembly Station

Hi

 

Can any one tell me why Plant Simulation Chrases when I Create a MU on an Assembly Station.

 

This is the command I use:

.MUs.Entity.create(Assembly);

 

See attached model

2 REPLIES

Re: Plant Crashes when I Create a MU on an Assembly Station

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi CavemanProgram,

 

we will fix this bug in our next patch release.

 

The reason why this wasn't detected yet, is that it would not work anyway. The assembly has to detect if a part is a main part or a side part. This is done by checking from which predecessor this part is coming, which cannot be done if the part is created on the assembly.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Plant Crashes when I Create a MU on an Assembly Station

Hi Ralf

 

Thanks for the quick answer. Im just happy that PS save the model before shutdown :-).