Cancel
Showing results for 
Search instead for 
Did you mean: 

Plant Sim 14 Chart Input Channel bug

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

When updating Input channel values, debugger keeps opening metioning an uninitialized variable. Names in the frame have been updated to match the channel input table but it doesn't refresh after until closing and opening the model.

 

To whoever may concern

2 REPLIES 2

Re: Plant Sim 14 Chart Input Channel bug

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you post a model, or at least a screenshot of the debugger?

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Plant Sim 14 Chart Input Channel bug

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I already solved the issue, if I got through it again I'll take screenshots of everything.