Cancel
Showing results for 
Search instead for 
Did you mean: 

Plant Simulation 12 vs. Plant Simulation 13 Student Version

Pioneer
Pioneer

Hallo,

 

I write my thesis, because of that i use  Plant Simulation 12 Version at work and Plant Simulation 13 Student Version at university.

 

When I create a model in Version 12 at work, i send to me and i can open in Version 13. However, i make changes in Version 13, I can not open it in Version 12 again.

 

Is it possible to save the model as earlier version? Or is there any other solution for this problem?

 

Thanks in advance,

Beril

2 REPLIES

Re: Plant Simulation 12 vs. Plant Simulation 13 Student Version

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello b_balkan,

It's not possible to open newer models in older version.

But the license file you have for version 13 allows you to use version 12 as well.

So you can just install version 12 in parallel to your computer using the installation medium of the University.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Plant Simulation 12 vs. Plant Simulation 13 Student Version

Pioneer
Pioneer

Hello Ralf,

 

Thank you very much for your quick reply. I will install version 12.

 

Regards,

Beril