Cancel
Showing results for 
Search instead for 
Did you mean: 

Plant Simulation 3D On-Line Training Excercise

Siemens Creator Siemens Creator
Siemens Creator

This message is intended for the participants of the 3D On-Line training

 

Please download the attached sample model (V11.05) and make the following modifications:

 

1. Replace the graphics of the Stations, Movable Units and Containers

 

2. Try using meaningful 3D data that you can share, else use graphics included with the software or 3D primitives

 

3. Change the path and graphic parameters of the conveyors (be creative here ! )

 

4. Add few interesting camera mark ups

 

5. You can add text notes and restrict access to the model, if you have been to this class as well !!

 

6. Send back the revised model

 

 

 

1 REPLY 1

Re: Plant Simulation 3D On-Line Training Excercise

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Good material.