Cancel
Showing results for 
Search instead for 
Did you mean: 

Plant Simulation connect to the OPC server failed

Pioneer
Pioneer

hi, I meet a new problem about the OPC .when I active the OPC_interface in plant simulation ,a imformationbox appear:

connecting to the OPC server failed:

CoCreateInstance({75D00BBB-DDA5-11D1-B944-9E614D00000})没有注册类

 

do you know how to solve this problem?

1 REPLY 1

Re: Plant Simulation connect to the OPC server failed

Siemens Phenom Siemens Phenom
Siemens Phenom

Did you install the "OPC Data Access 3.00 Core Components"?
You can find them on the installation DVD or in the zip file that contains the setup.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.