Cancel
Showing results for 
Search instead for 
Did you mean: 

Plant Simulation for 3D Printing/Additive Manufacturing

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello Community,

 

I am wondering if anyone has created a model of an additive manufacturing/3D printing process? I think it's an intriguing idea and I am trying to wrap my head around if there are any obvious pitfalls to modeling such a process or if it can be regarded as a straight forward "discrete MU" process?

 

My main thought it how to handle powder/raw material and how much is consumed by parts 3D printed. Would it be most practical to use the fluid objects/portioner or is it enough to fill a buffer/set a variable to an amount of raw material which is "subtracted" depending on how much is required to produce a specific part? I.e. a fluid -> discrete process, or purely discrete process?

 

Another thought is how to handle the 3D printing machine itself. Can it be simplified to a procTime or are there other parameters to consider (except loading, unloading etc.)? It seems impractical (albeit dynamic) to calculate a proctime from the feed speed of the machine and the part dimensions/volume.. This would also produce the amount of raw material required from the storage, but again it seems complex to calculate this for each part to be produced.

 

Does anyone have any experience in this area and shed some light? I'm trying to brainstorm some ideas.

 

Thank you!

 

3 REPLIES

Re: Plant Simulation for 3D Printing/Additive Manufacturing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
I guess you need to set some priorities.

If you follow the "material flow" idea, the 3D printing is a source. You can easily create a delivery plan. The consumption of material you can trigger by the exit control (if this is not the priority).

If you want to model the occupation of the printer (e.g. based on the "printing speed e.g. in kg/hour") than indeed the portioner could be a good way. You can change the amount of material for the MUs with amountPerMu (e.g. exit control based on a plan).
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Plant Simulation for 3D Printing/Additive Manufacturing

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Steffen,

 

Thank you for your insight.

 

For modeling production line throughput depending on amount of workers + number of printing machines, I guess the occupation of the 3D printer would be necessary to model with the help of the portioner?

 

In a case I am looking at, the occupation of the printer is of interest due to it affecting other things in production, but the consumption of material wouldn't have to be in such great detail. I guess the portioner would be a nice way to get Plant Simulation to automatically handle the consumption of raw material but I am unsure if this way is more complicated than , for instance, manually handling material consumption by decrementing a variable in an entrance/exit control.

 

 

Re: Plant Simulation for 3D Printing/Additive Manufacturing

Experimenter
Experimenter

Hey 7SEG,

 

I'm happy to read, that you are also thinking about the specifications of a additive manufacturing process and the way of implementing it to PlantSim.

At the moment I try to model a Maintenance Center for the production of spare parts and have problems with the layout and the material flow. Since your post is already more than a year ago I would like to know, wheter you may have already finished you model and could share your experience/ results with us?

 

Thank you in advance!