Cancel
Showing results for 
Search instead for 
Did you mean: 

PlantSim demo version and interface examples are not working?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

In PlantSimulation a lot of demo examples are provided. I'd like to run all the interface demos. However, it seems to be a license problem. In the console it is written:

 

>>>license emplant_ifpack is missing.

 

or, text in german (because a german PlantSim is running)

>>>Fehler in Methode '.Models.ActiveX.AccessingXL.startExcel' in Zeile '6': Lizenz 'emplant_ifpack' nicht vorhanden.

 

Where to get that license?

12 REPLIES 12

Re: PlantSim demo version and interface examples are not working?

Siemens Phenom Siemens Phenom
Siemens Phenom

You're right, many of these examples need the Plant Simulation Interface Package.

This is a license option which can be bought in addition to the general Plant Simulation license.

It has the product id TN75050. You can contact your sales representative to get a quote.

 

In case you are using the student license, you unfortunately don't have access to this license option.

 

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: PlantSim demo version and interface examples are not working?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Thank you for the quick answer.

 

regards,

Franz

Re: PlantSim demo version and interface examples are not working?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Please let me add a question:

 

actually I'd like to create a prototype which should demonstrate a communication of PlantSimulation with our tools. PlantSimulation offers a lot of interfaces, e.g. TCP socket, com, ODBC and OPC are the prefered one.

 

Now the question:

Is it possible to run the demo-version in combination with the "interface package license", and will the interfaces become working ?

 

Thank you for answer.

regards,

Franz

 

Re: PlantSim demo version and interface examples are not working?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Franz,

 

when you talk of the demo-version, do you refer to the free viewer license or our free trial license?

 

The free viewer license should not be able to import or export data. Even if you have the interface package license you cannot use it with the viewer license.

 

For the trial license we have decided that the interface package is not important for doing an evaluation of the product.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: PlantSim demo version and interface examples are not working?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Well, hard to say. It seems to be a trial version.

After registering at your homepage I got an email with the license file. Here it is described:

>>>Thank you for downloading the Tecnomatix Plant Simulation trial version.

>>>Included in this email is the license file to activate your Plant Simulation 30-day trial.

 

In PlantSimulation tool at the menu configuration - license - it is written:

   kind of license: Educational

 

 

In the license-file byself it is written:

# --------------- ----- --------------------  ----- ---------------------------
# TN75040             1 Plant Simulation Edu      1 emplant_edu                 
# TN75096             1 VSM Library NL            1 emplant_vsm

 

Is it meaningfull to combine the "interface package license" with my product?

Re: PlantSim demo version and interface examples are not working?

Siemens Phenom Siemens Phenom
Siemens Phenom

This is the trial version.

 

As mentioned above the interface package is not available for the trial version.

We assumed that no one will have time in the 30 day trial period to dig into our interfaces.

 

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: PlantSim demo version and interface examples are not working?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Ok. Good to know.

 

As already posted before,  the trial version contains a lot of examples (models) to demonstrate the interfaces, e.g. Excel import/export.

However, now it's fact that in the trial version they can't be started.

 

Would it be possible to add a hint in the documentation, could be in the next PlantSimulation version.

 

regards,

Franz

Re: PlantSim demo version and interface examples are not working?

Siemens Phenom Siemens Phenom
Siemens Phenom

Good Point.

 

We will discuss this and either add a hint or add the interface package to the trial license.

 

Thanks,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: PlantSim demo version and interface examples are not working?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

We had in mind to use the trial version for an OPC connection-test with PlanSimulation and one of our devices.

As noted before in the posts the trial version can't be used to test the OPC connectivity.

 

So, please let me ask a detail about your OPC version:

 

PlantSimulation 11 supports OPC DA client 2.0

Now, our devices runs a OPC DA server 2.05a

 

Is a connection possible ?