Cancel
Showing results for 
Search instead for 
Did you mean: 

PlantSimulation Export & Import vis XML is not properly handling subtables and formulas

Builder
Builder

Hi!

 

I was exporting tables with subtables (cascaded two times) via XML. Importing those tables into another PlantSimulation model configured the different column properties as they have been before, but the subtable configuration in the format area was not adapted at all.

 

In addition colums with formulas were not handled properly. Neither the formula nor the result value was transferred.

 

Finally the column width are ignored in every case.

 

Can this be fixed/adapted in the future?

 

Thx,

Mak

1 REPLY

Re: PlantSimulation Export & Import vis XML is not properly handling subtables and formulas

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Mak,

 

the XML data format wasn't intended for export from and import into Plant Simulation.

 

For this purpose the table should be exported as an object file.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.