Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Poblem with seed values of experiment manager

Creator
Creator

Hi,

I opened a model from version 10.1 in version 11_TR1.

I tried to run the experiment manager but had some problem with the seed values.

I wonder if somebody faced the same issue.

attached the error screen.

Thanks

Shai Weinbren

6 REPLIES 6

Re: Poblem with seed values of experiment manager

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Shai,

 

from V10.1 to V11 the random number generator was simplified significantly.

 

This required some code changes in the experiment manager.

 

The problem should be resolved when you update the experiment manager library in your model to the most current version.

You can do this in the Library Manager.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Poblem with seed values of experiment manager

Creator
Creator

Thanks for your reply.

I updated the libraries but still got an error (see attached file).

In addition, I do not see in the new updated Experiment manager the options of configuration method & Evaluation methos which enabled input and output of data during runs.

Thanks in advance

Shai Weinbren 

Re: Poblem with seed values of experiment manager

Siemens Phenom Siemens Phenom
Siemens Phenom

The methods you mention can now be configured in the 'Advanced Settings...' dialog which you can open in the 'Tools' menu of the Experiment Manager.

 

We moved them since for a beginner it was very confusing to know what had to be entered to configure an experiment.

 

It seems that you are using an user evaluation method which is coming from a previous version which expected only two parameters.

Now this methods expects three parameters: (localExp,localRun,localObserv:integer)

 

You have to change your user defined evaluation methods accordingly.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Evaluation Method

Creator
Creator

Hi Ralf,

Thanks for your help.

I tried to change the parameters with no success.

Attached my: evaluation method.

I will appreciate if you look and see what needs to be changed.

Thanks

Shai Weinbren

Re: Evaluation Method

Siemens Phenom Siemens Phenom
Siemens Phenom

You have to change the parameter declaration in your method from

 

(CurrExp,CurrRun:integer)

to

(currExp,CurrRun,localObserv:integer)

The custom evaluation method now gets an additional argument where you can see in which observation you are.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Evaluation Method

Creator
Creator

Ralf,

Thanks.

Shai Weinbren