Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Point Cloud- e57

Pioneer
Pioneer

Hi,

I have a point cloud in E57 format, is it possible to import E57 files into plant sim? or is the .pod file required?

many thanks for your help.

2 REPLIES 2

Re: Point Cloud- e57

Siemens Phenom Siemens Phenom
Siemens Phenom

Plant Simulation can only read .pod files so you will have to create one beforehand out of the E57 file.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: Point Cloud- e57

Pioneer
Pioneer
great thank you