Cancel
Showing results for 
Search instead for 
Did you mean: 

Point cloud samples

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Forum

 

Since Plant Simulation has the capability of importing point clouds, I was wondering if anyone knows of freely available sample files to test it out?

 

Regards,

Hermias

2 REPLIES 2

Re: Point cloud samples

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Hermias,

 

the problem with point clouds is that they are usually very big.

 

The free one we have is 8GB. It was distributed on the user meeting last year.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Point cloud samples

Legend
Legend
Hello,

It is possible de make it available on the website to download it ?

Thank you Hermias !

BR
O.C