Cancel
Showing results for 
Search instead for 
Did you mean: 

Portal Crane .moveHook(x) not displaying in 3D

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Forum

 

I've experienced  in multiple models (even the sample models) that when calling portal.movehook(x), the hook's position does not update in 3D.

 

Has anyone experienced this before as well?

 

Regards,

Hermias

2 REPLIES 2

Betreff: Portal Crane .moveHook(x) not displaying in 3D

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Hermias,

 

the hook does not move, if the value for the position is out of the range of the hook.

Therefore the method moveHook provides a result, showuing if the hook can be moved or not.

Please check this.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Portal Crane .moveHook(x) not displaying in 3D

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks GG!

I updated the portal Method to have a check at each movehook command:
local check := portal.moveHook( 2 );

I saw that if you attempt to move a hook to the same height as the portal, it returns false and does not move.
If it is below the total height of the portal it works 100%.

If I however change to height of the runway to represent a crane working on beams in a ceiling and the portal height to 0, it does not work.

What I realised is that the height of the portal itself has to be more than 0 for the movehook(x) command to function properly.