Cancel
Showing results for 
Search instead for 
Did you mean: 

Portal crane Mu Pickup

Experimenter
Experimenter

Hi Everybody, 

I have two questions regarding the usage of the portal crane and Storage area. 

1. Is it possible to set the "resting position" of the portal crane

2. In my model, i have my portal crane pickup mu's from the storage area and drop them off on a conveyor (trough a buffer). Is there a command which allows me to let my crane pickup a mu from the storage area, steer it to the conveyor, hover over it, and only on a different command let drop the mu's off at the conveyor? 

 

Thanks in advance! 

Greetings

1 REPLY 1

Re: Portal crane Mu Pickup

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

1. insert a (dummy) object for the waiting position, then you can move the crane to this object

2. move the crane to the object (may be you need a drop point as a object, if the positioning is not working), lower the hook and move the MU using SimTalk move from the hook to the conveyor (see help moveHook, moveToObject)

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net