Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem in Carry Part Away

Pioneer
Pioneer

Good morning folks.

I am developing a project, and in one part of it there are two machines and a 'worker' manually carries the play from one to the other. For this using the 'Exit Strategy', 'Carry Away Part'. Until then it's all right. It turns out that I have saved shifts in 'ShiftCalendar'. When the 'worker' is carrying the piece and the work shift ends, the 'Worker' do not let the play on the machine and walks away with it until the WorkerPool, making the program give error.

Any suggestions for my problem?

The problem occurs at the time '64: 09: 14: 10. '

I am sending the file ...

2 REPLIES 2

Re: Problem in Carry Part Away

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello Martins,

 

Please check the Help Documentation for the "Part Buffer" field of the Worker Pool.

 

Sincerely,

 

Re: Problem in Carry Part Away

Pioneer
Pioneer
Thanks Sebastiaan.
Your help was very useful.