Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem running the simulation!

Creator
Creator

hello friends!

Why does Transporter quickly move from the beginning of the track to the end and enter the next object connected to the track?The certain process on the track is invisible at all

6 REPLIES 6

Re: Problem running the simulation!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

what are you expecting?

The track is passive, by default there is no "process" on the track.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Problem running the simulation!

Creator
Creator
hi Bangsow:
Thanks for the quick response. What I mean is that even if my simulation speed is very slow, the Transporter moves very fast on the track and seems to move from beginning of the track to the end momentarily.

Re: Problem running the simulation!

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello James,

 

if you set your simulation time to "Real-Time" your transporter should move smoothly on the track.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Problem running the simulation!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
ok, in this case you need to check the connectors (is one above the track?), check the length of the track and the speed of the transporter; if you use an icon with an animation line, you need to set a sufficient numbers of animation event...
There can be different reasons for this behavior; hard to say without to see your model.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Problem running the simulation!

Creator
Creator
hi Igor:
Thanks for the response. I have set my simulation time to "Real-Time" before I started the simulation.

Re: Problem running the simulation!

Creator
Creator
Ok,I will try your suggestions.Thank you !