Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Crossing Line

Pioneer
Pioneer

Hi everyone,

I just start to learn how to use crossing Line on plant simulation.

I try the example on tutorial but I have the problem ( the programm stops after a few moment when I execute it).

This is the model can you help me please to resolve the problem?

Thanks for your help

2 REPLIES

Betreff: Problem with Crossing Line

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Manu15,

 

in your  simulation model, the method partHere is also defined as an Entrance Control of object Line2.

This does not make any sense. Remove the entrance control of line 2 and your model is running as expected.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Problem with Crossing Line

Pioneer
Pioneer
Thanks GG