Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with MUs stuck in a buffer

Creator
Creator

I need some help with MUs stucking in a buffer. 

The model I created uses buffers to put the MUs in a sort of 'packages' having certain number, to simulate that the machine starts only when it is fully loaded. After processing about 95 objects the MUs got stuck in a buffer (Ringowanie2) AND the machine (Maszyna 2), because of what whole system stops.

How can I 'push' the MUs out of the machine to create space for the items from the buffer? Or is there another solution?

 

I attatch the model for deeper understanding. 

2 REPLIES 2

Betreff: Problem with MUs stuck in a buffer

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi PiotrekO,

 

can you send the model?

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Problem with MUs stuck in a buffer

Creator
Creator

Sure, I thought I have already done that. My mistake.