Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Transporter Routing

Valued Contributor
Valued Contributor

Hello I have modeled a gantry using a transporter. The problem i am encountering as of now is with respect to the destination where the transporter needs to be routed. If the desired destination of the Transporter is object A, the transporter takes some other destination when the sensor in the track corresponding to the object A is triggered and the transporter remains still as the control will not get executed. Can anybody help me out to eliminate this problem so that the transporter takes the desired routing.

 

Thank you

1 REPLY 1

Re: Problem with Transporter Routing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
hard to say without your model, but to use the routing you need to do two things:
- connect the sensor with the object (setting: only if destination --> set the destination)
- set the destination attribute in the transporter (before you start)

The transporter will stop only automatically (and call the sensor control), you need to set the direction and start the transporter by SimTalk.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net