Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with importing external models into PlantSim 3D

Experimenter
Experimenter

I'm a new learner for plantsim 3D, and I have some critical error while trying to import and save external models from solidworks. These steps are followed: (My version is 11.3 64bit)

1. Translate solidworks model into *.vrml

2. Duplicate a SingleProc, rename as Mymachine, and select "open in 3D". Delete the original 3D model, and use "import graphics" to import my model. 

3. Setup animation path and graphic groups

4. Save Mymachine in obj.

Then problem occurs, when I try to load this object, a critical error appears as:

Error.png

Then , all the 3D model and animation details lost. 

Besides, I've tried Jt and vrml. Both have the same problem. My models are attached. 

Can anyone help me figure out what is wrong?

 

Thanks in advance!

2 REPLIES 2

Re: Problem with importing external models into PlantSim 3D

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Hann_Yu,

 

I tried to follow exactly your described steps and it works just fine, see attached file.

 

Which patch level of V11 are you using? The latest version is 11.3.3.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Problem with importing external models into PlantSim 3D

Experimenter
Experimenter

Hi, Ralf. Thanks for your reply. 

 

My old version is 11.3.0. I update the version to the latest, and it's OK too. Smiley Happy

 

Cheers