Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Problem with project

Pioneer
Pioneer

Percentage is related to Length*Width, because it’s percentage area.
So its not important where I will cut elements on the sheet, I want only have something like that:
SHEET.png

Re: Problem with project

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

so you can change the MULength attribute depend on the MU-Name in the exit contol (rear) of the DismantleStation. If you activate the vector graphics in the MU (tab graphics) also the representation of the MU change depend on their length, see the attached example.

 

waste.png

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Problem with project

Pioneer
Pioneer

This is what i meant, but now i have one type of waste. What if I want to have for each type of sheet , another percentage of waste? The type of sheet i can implement from tablefile, can i do that with waste?

Highlighted

Re: Problem with project

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you could define the waste percentage as user defined attribute of the sheet. You can set the values with the creation table of the source. In the entrance control of the DismantleStation you can set then the ratio for the waste for each kind of sheet (and read this value in the exitControl).

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Problem with project

Pioneer
Pioneer

Ok, I will do that. Thank you.

Is the possibility of incorporation FlowControl to Method?
Because in my model I have crane., which moves elements from quality_control do flowcontrol.
Then flowcontrol moves automatically elements to elements_magazine or refuse.
And I would like to crane raised elements form quality_control and moves 98% elements to elements_magazine and 2% to refuse. And the second situation if waist have 10%-50% area then go to refuse and when have 50-90% sheet_magazine.

Re: Problem with project

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you can select the Exit Strategy Method, the method needs to return the successor number.

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Problem with project

Pioneer
Pioneer

Thank you very much for early help.

I have a question, how can I make in the method, that shared a percentage (98-2%)
In first FlowControl I used “If…” everything works but it should look like a command to the division of percentage?
rysunek1.png

And my sencend question. I try to use Ratio in Wycinarka (Cutter) and I use method and I use the method at the exit and entrance. But something is wrong and isn’t divided into parts.
rysunek2.png

Re: Problem with project

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you can use the method z_uniform to dice a value between 0 and 1.

So you can create a condition like this:

 

local rand:real;
rand:=z_uniform(99,0,1);
if rand <= 0.98 then
--98%
else
-- 2%
end;

What is your setting of the DismantleStation (the attachment is the wrong file)? You need to create a new part (waste) then you only set the MULength in the exit control. Depend on the names of the MUs you can split the materialflow in a exit control (front). 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Problem with project

Pioneer
Pioneer

This Method is very helpful, thank you.
But I still don’t understand, how I can divide.
I have e.g. that situation:
Two different plate: Plate and Plate2, First Plate I use 60% so I have Waste=40% and Component 60%
and Plate2 I use 10% so I have Waste=90% and Component 2 = 10%
WasteRatio I have permanent , so I should take WasteRatio in tablefile in column Ratio? And open inside table and put it inside or  I can’t do it that ?  

photo.png
And I should change “changeLength” ?
photo2.png

Re: Problem with project

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This is the right way to define the wasteRatio as attribute in the plate. But you should insert the value in the column real (this is the right data type).

 

To take into account different ratio values, you need an entrance control in the DismantleStation.

 

waste1.png

 

For Divide into Component and Waste you can use the DismantleStation. It creates additional to the Plate one piece waste. If you change the MULength of both, you can later read this value and make a decision, if you can reuse the waste as new (shorter) plate or not. If you have to reuse the waste, it may be better to have an absolute value for length/width for the component insead of a ratio to select the right plate.

 

For devide the materialflow you can use the MU attributes name and MULength.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net