Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with the loading of MUs on wooden palets

Experimenter
Experimenter

Hi everybody ! 

 

I want to generate MUs on palets, together on a conveyor, but with the ONLY use of a method, and no PaP robot.

 

The problem is that i already have two sources with a PaP robot, and when i try to generate new palets with the method, it changes the parameters of the first palet. 

 

For example, I have one MU, one palet and a conveyor. I would like to generate a fully loaded palet with my MUs on it. 

 

thanks a lot in advance for your help ! 

 

 

 

 

 

 

3 REPLIES 3

Re: Problem with the loading of MUs on wooden palets

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
can you post an example ?
create returns a link to the created pallet, with the link you can change the attributes; if your case it sounds, that you are set the attributes in the class of the pallet, this would be wrong
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Betreff: Problem with the loading of MUs on wooden palets

Phenom
Phenom

Here's an example on how to load the entitys

 

Unbenannt.PNG

Betreff: Problem with the loading of MUs on wooden palets

Experimenter
Experimenter

Hi, 

 

Sorry for the late answer, didn't find the time to work this project since last week..! 

 

Thanks a lot for your solution, I tried and it worked perfectly !!! 

 

Problem solved ! 

 

Once again thank you ! Smiley Very Happy