Cancel
Showing results for 
Search instead for 
Did you mean: 

Process Simulation of a Milk Seperator

Experimenter
Experimenter

How do I simulate a process the actually takes a product such as milk and split it into "cream" and "Skim" milk. I would also like the option to include a cleaning cycle within this asset. The flow into the milk seperator could be variable as it would be controlled by a valve.  Does anybody have a libary?

1 REPLY

Re: Process Simulation of a Milk Seperator

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have one example from my new book:

 

http://www.bangsow.de/detail_en.php?id=684

 

The "old" stream is deleted by a fluid drain and two sources produce the new materials. With the help of SimTalk the Sources only produce, if there is fluid in the incoming pipe.

 

fluids_separator.gif

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net