Cancel
Showing results for 
Search instead for 
Did you mean: 

Processing times matrix

Hi Sim Superusers,

 

I need to create a matrix for proc times based on MU and Machine more like a setup time matrix table. So that I can have one table with all MUs listed on column 1 and all machines listed on rows, and machines will read proc times from table based on MUs and Machine combination. Any suggestion on this item? 

 

Thank you!

 

Karthik Murugan

1 REPLY

Re: Processing times matrix

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

the best would be to write the MU-names in into the column 0 (row index), machine names in col index (row 0)

 

then you can set the procTime using the setting formula

 

matrix[?.name,@.name]

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net