Cancel
Showing results for 
Search instead for 
Did you mean: 

PullCtrl / fwBlockList

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello,

 

is it possible to track the fwBlockList?

 

I'm using my "own" PullCtrl within a buffer, to control which object should be processed (FIFO).

By

tBlock:table; n: integer

 “buffer.unblock(tBlock [1,n])” --(n=1 , fwBlockList.ydim>1) ,

 

the first object should be unblocked an then move to the buffer, but in some cases the second entry disappears and the correspondent object remains on its position.

 

any idea?

Thanks TO

5 REPLIES

Re: PullCtrl / fwBlockList

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi TOpp_Sim,

 

it might be that the exit control of a previous station move the wrong part to the wrong station.

 

The method 'unblock' which you use, just inserts a new out event for the part.

 

If you use an exit control in the station where the part is located you have to have the following:

(demandingStation:object)
is
do
    if demandingStation /= void then
        @.move(demandStation);
    end;

    .
    .
    .
end;

 Otherwise it might happen that the part is unblocked by station A and then moved to station B.

Also make sure that you always move the active part (@) in your exit control.

 

Of course all this assumes that you have an exit control.

In case you don't have one, the model would be helpful to debug what's going on.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: PullCtrl / fwBlockList

Phenom
Phenom

Hi,

 

w/o a model ( either yours or own redesigned model ) it becomes more or less a guessing, what led to your described scenario.

 

In these kind of cases and in any cases where there are doubts about the model behaviour  I strongly recommend to use the eventdebugger ( s.button in eventcontroller dialog below ).

 

With the eventdebugger ( no programming ! ) you can easily step through the eventlist and monitor every single computed event.

 

Once used, the model behaviour should become transparent.

 

xxx.JPG

Re: PullCtrl / fwBlockList

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Ralf,

sorry the model is very complex and large, so I can't attach it.

Debugging wasn't successful.

 

My part (ord:1759) can't move to its destination (self developed modul) by method, because of less capacity, enlists in the fwBlocklist and waits on its "new" out event, triggered by destinations pullctrl. 

The pullctrl always unblocks the first entry. But "suddenly" the second entry (ord:1759) disappears without triggering a new out event for correspondent part (ord:1759).

 

BL.jpg

 

 Neither the eventcontroller nor the log file gives an indication of what happens and why.

 

By now I found a solution for the problem, but no answer to the question. Woman Frustrated

 

Regards,

Tanja

Re: PullCtrl / fwBlockList

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You you have some waituntil connected with moving parts (esp. with using of @) upstream of this station? This sounds like a supended method wich moves the part (no event - I guess moved by method).

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: PullCtrl / fwBlockList

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Steffen,

I allways try to avoid using waituntil-constructs, because of "unmanageable" suspended methods in large models.

I know, why the part doesn't move to its destination, but I can't find out what makes the pullctrl choose the wrong part, respectively choose the right one ( degugging the method) but "take" the second one.

 

Regards

Tanja